MOVE.INPOSLIMIT

Description

Specifies the tolerance of Position Error (PL.ERR) within which the MOVE.INPOSITION flag will be set to 1 (True). Set MOVE.INPOSLIMIT before using MOVE.INPOSITION.


  • MOVE parameters are only valid when DRV.OPMODE = 2 and DRV.CMDSOURCE = 5.

General Information

Type

R/W

Units

16 bit counts

Range

0 to 140,737,488,355,328

Default Value

0

Data Type

Integer

Variants Supported

This parameter is only supported on AKD BASIC drives.

Fieldbus Information

Fieldbus

Index/Subindex

Is 64 bit? Attributes Signed?

Object Start Version

Modbus

1114

Yes 64 bit Yes

M_01-05-11-000

Related Topics

MOVE.INPOSITION